Cancel
Showing results for 
Search instead for 
Did you mean: 

Midplane feature in the new release ?

Pioneer
Pioneer

Hi All,

 

do you know whether that function as Midplane will be implemented in the new SE version ?

 

I personally need it .... instead of measuring the distance between two bodies and cereate the plane ....

 

Thank you

 

Arek

 

 

Solid Edge ST8 MP10
8 REPLIES 8

Re: Midplane feature in the new release ?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Arek:

 

No mention in the ST 9 beta PPT with 153 slides and nothing found in the ST 9 beta help either.

It just might make it into the final release, since beta is different from the final release.

 

~Tushar

 

Re: Midplane feature in the new release ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@ArekK Can you explain the root reason for a mid plane between two faces?  Perhaps there is another way to achieve what you are after.  I'm sure you are aware that when placing a parallel plane, you can dynamically place the offset and can locate element midpoints.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Midplane feature in the new release ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I'm assuming the issue is that if you want a plane to always be halfway between two faces even if the two faces change now you need to do it with variables or a sketch entity. It would simplify the process if SE did it for you.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Midplane feature in the new release ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This has come up before:

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Plane-between-to-solids/m-p/324956/h...

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Midplane feature in the new release ?

Honored Contributor
Honored Contributor

With sheet metal, There is an option to make normal cuts from the mid plane. So there already is some coding to deal with the mid plane.

 

The one I'm looking for is the K plane and cuts from the K plane.

Note: K plane = neutral axis for sheet metal.

Re: Midplane feature in the new release ?

Pioneer
Pioneer
@KennyG - Hi, Using midplane and its feature in for example 3 clicks as it is in Solidworks would bring us a lot of saved time to mirror parts, create new ones etc.

So far I have to : ( in steps ) measure the distance, create a plane ( sometimes I have to create a plane before measure the distance ), and then create another plane as a midplane, then do mirror or create another part .

for me waste of time in fast paste environment.

Thank you,

Arek
Solid Edge ST8 MP10
Highlighted

Re: Midplane feature in the new release ?

Pioneer
Pioneer
Hi,
I checked it before a post my question.

Regards,
Arek
Solid Edge ST8 MP10

Re: Midplane feature in the new release ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What's about a 3D sketch betwen the two bodies and a plane (coordinate sytem) at the midpoint of it?

 

 

regards
Wolfgang