Cancel
Showing results for 
Search instead for 
Did you mean: 

Migration from ST6 to ST7

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Hi All,

 

I know this question comes up about every 6 months, and I know I have seen something recently from Dan Staples about how to do this, but what I would like to do is to keep all the settings and customisations from ST6 and migrate them to ST7.

 

Ideally for me, any user opening ST7 would have a similar experience as they did in the ST6 predecessor. I know there have been improvements, but I could really do with out the month of whinging that seems to follow an upgrade.

 

Any help (search suggestions will be welcomed as well, I have tried a couple and have not come up with anything) will be greatly appreciated.

 

It is a shame there isn't an upgrade wizard yet, that lets you migrate what you need to, while still being able to see what is new.

 

Shane

Shane Murray
SE2019 MP3
4 REPLIES 4

Re: Migration from ST6 to ST7

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

You unistall ST6. You then install ST7. When opening ST7 for the first time, it will migrate your setting from ST6 over. There's some thing you have to re setup like your file locations. That's about it. rest of it you have setup your self, Background color, Pathfinder and ect.  Now once you setup one computer and want to set the rest up little faster. let me know

Re: Migration from ST6 to ST7

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I guess it would be quite good to replicate my settings on other machines. However it looks like a couple of weeks of complaining is the way to go...

Shane Murray
SE2019 MP3
Highlighted

Re: Migration from ST6 to ST7

Phenom
Phenom

Try copying this folder from your existing machine to the same location on the new machine -

 

C:\Users\[your username]\AppData\Roaming\Unigraphics Solutions\Solid Edge\Version 106.

 

When you start ST7 it should then use these settings as previous posters have shown.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Migration from ST6 to ST7

Pioneer
Pioneer
As beachcomber states, copying the folder is a good idea.
There are about 6 "personalization" files that should be copied over for each machine. Things such as custonized color layouts, callouts, BOM settings, etc can be retained from one version to the other. Remember that each machine should have these copied from the local drive. I oversee 6 seats here where I work.
Greg Patchel
Win 7 SP4 64 Bit
HP Z400 ST7 MP4
16GB RAM 3.2GHz
NVIDIA Quadro 2000

There are two kinds of people, those that can extrapolate from incomplete data...