Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Migration hole tool from SW to SE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi mates!

 

I was wondering if any os you can tell me how to use the tool SEHolePipeTxtFromSW.exe, with an example or a screenshot of the use of this tool please,  because I’m reading the help of Solid Edge but it’s not clarified in the way of typing the required information in DOS. 

 

Regards!!

2 REPLIES 2

Re: Migration hole tool from SW to SE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Joanpolo  Based on the ST10 Help, it appears there are 4 arguments to the SEHolePipeTxtFromSW.exe command:

  1. "Holes" or "Pipes"
  2. Path/Filename of the SolidWorks "SWBrowser.mdb" file
  3. Path to save the Solid Edge "hole.xls" or "pipe.xls" file
  4. The unit standard to convert (Help shows the codes to use)

So I would imagine the syntax to be:

 

SEHolePipeTxtFromSW.exe Holes c:\folder1\folder2\SWBrowser.mdb c:\folder3 ai

 

This would convert the ANSII Inch holes in the SolidWorks database to a hole.xls file in c:\folder3.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Migration hole tool from SW to SE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi @KennyG , thank you very much. 

 

I was using the syntax as it is in the program, with this []

 

Now it works Smiley Happy

 

Regards