Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirror and Delete Features

Creator
Creator

I am looking to flip one feature (a cutout and holes) from one side of my part to the other, and then delete the initial feature.  In sketching there is a "copy" feature that you can turn on and off to do this, but is there a similar way to do it for cuts, etc?

8 REPLIES

Re: Mirror and Delete Features

Valued Contributor
Valued Contributor
could you provide a model ? or image ? You can mirror features in synchonous.

Re: Mirror and Delete Features

Creator
Creator

I would like to put the cutout and two holes on the side with just the cutout and vice versa.

Re: Mirror and Delete Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

To reiterate, is it synchronous or ordered?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Mirror and Delete Features

Creator
Creator

Synchronous

Re: Mirror and Delete Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think you could mirror them or select and rotate around the axis with the steering wheel.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Mirror and Delete Features

Creator
Creator
If I mirror is there a way to delete the initial features at the same time?

And when trying to rotate them around with the steering wheel it says Change the Design Intent settings or command options and try again.

Re: Mirror and Delete Features

Creator
Creator
I can, however, rotate the rest of the cylinder to get the desired result I still would like to know if there is a mirror and delete original for features.

Re: Mirror and Delete Features

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can turn off live rules if you need to. And you can always try things and undo or quit without saving.

And yes, usually you can mirror and delete the original.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200