Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirror feature command (Ordered) not recognizing pattern

Pioneer
Pioneer

I am trying to mirror a pattern of rectangular strip extrustions about a mid-plane. I have tried using both smart and fast mirror options.  I have no problem selecting the pattern, but when I  select the plane,  no mirrored feature results. I am certain I am doing this correctly, but obviously have encountered something new. 

 

I upgraded to ST10 MP3 yesterday.

 

My laptop is an MSI WT70-2OK with an i7-M4810 chipset running Win10 Pro and using an Nvidia Quadro K-3100 GPU.

 

Thanks!

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8
17 REPLIES 17

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @jstockton,

 

I this case you are mirroring the actual body not just features on a body, so you might try using the sub-menu command "Mirror Copy Part"..... hope that helps.

 

 

ST10_PAR_Ord_MirrorCopyPart.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Mirror feature command (Ordered) not recognizing pattern

Pioneer
Pioneer

Hi Sean

Thanks for the quick response.

 

The screen shot I used was misleading - I intended it only to show the model and what I was up against. I'm uploading the image of working within the part itself and trying to mirror the original strip as well as the array and the 1st mirrored image. 

 

As you can see the original strip is the only feature that gets mirrored. However, the construction consists of the original strip on the bottom left corner which is patterned and then mirrored about the x-z plane. I want to mirror the entire group about the y-z plane now, but this is where the error is occuring. The error I get is "some of the resulting features do not add or remove any material"

 

Thanks for your thoughts,

 

John

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @jstockton

 

 

at the moment I only can assume some reasons.

 

For me, it looks like that there are multi bodies within Your part and the base body (plate) seems not to be the active one. I can imagine that a mirror of a cutout and patter in empty space will not work as long as tehre is nothing from where You can cut.

 

But this only is a feeling when look onto Your image

 

 

regards
Wolfgang

Re: Mirror feature command (Ordered) not recognizing pattern

Pioneer
Pioneer

Please see updated image for further clarity. I know I must be missing something but with 10 years on SE I can't figure this one out. it should be easy.

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Phenom Gears Phenom
Gears Phenom

I dont know it worked for me.

worked.JPG

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Phenom Gears Phenom
Gears Phenom

can you share your native SE file...   even if you need to obscure the original base profile and other features...    but let us take a hack at the real model as you see it regarding the mirror command.
???


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@nominus38, did you try it with the ends on the plane, then mirror the whole set over at that plane? ...I get errors using Mirror Copy Feature, until using Mirror Copy Body, at least, in that scenario.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Mirror feature command (Ordered) not recognizing pattern

Pioneer
Pioneer

Hi Sean,

 

That solved it! It was right under my nose but I didn't see it - thanks for identifying that option.

 

John

MSI WT-70 2OK;
Nvidia Quadro K3100M
WIN10 1709:16299.461
SE ST10 MP8

Re: Mirror feature command (Ordered) not recognizing pattern

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Most welcome John [@jstockton]

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000