Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirror of whole body within part (Ordered)

Creator
Creator

Hi all!

 

I am new to Solid Edge and to the forum, I am about to complete my first part modeled with SE, but I am struggling on mirroring the body I have designed.

 

Is there a way to mirror the whole body with respect to one ot its faces?

 

I have tried o use the "Mirror Copy feature" command, but it looks like I have to manually select all the features that made up the body: that is pretty difficult and error-prone.

 

Thanks in advance for your help.

2 REPLIES 2
Highlighted

Betreff: Mirror of whole body within part (Ordered)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @NicolaR

 

 

no problem at all.

Just use the Blue Mirror function rather than the Yellow one.

 

 

20181220_1140.png

 

 

This mirror function always is to prefer before the mirror feature command.

You will see, that using this one will keep the part size smaller, and will increase the performance for those parts.

 

 

regards
Wolfgang

Betreff: Mirror of whole body within part (Ordered)

Creator
Creator

Hi @hawcad,

 

thanks for that!

 

I tried the blue function at first, but I eventually couldn't reach the desired result... and then I have just kept trying to get the result with the feature command -.-'