Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirror

Genius
Genius
10 REPLIES

Re: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It doesn't seem like all features are being selected for some reason. Can you try it in ordered?

Always a good idea to upload the file here. Especially when it's such a small one.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Mirror

Genius
Genius

It works in Ordered.

 

 

Geir Ramstad

Solid Edge ST10 MP6

Solid Edge 2019

Betreff: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

 

You can see in Your video that even although t

You do a box select and all surfaces are shown green, the two base features (cylindars) in the pathfinder are not shown as selected.

Select them too and the mirror will work

regards
Wolfgang

Re: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

OK, the problem is the thread feature. For some reason when that's picked, like with a window selection, the thread can't be mirrored but it also leaves out the protrusion on which the thread is based. You should have gotten an error pop-up. So just pick everything except the thread in the pathfinder. But it seems you can't apply another thread to that new cylinder for some reason.

Also you can't mirror sync features in ordered but you can do "mirror copy part" which does take the thread.

That might work for you too.

edit: I see you discoverd the mirror copy part.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

 

here is the picture from above:

 

20180407_2219.PNG

regards
Wolfgang

Betreff: Mirror

Genius
Genius

I have selected all the features incl. thread.

But the thread will not copy.

Solid Edge 2019

Betreff: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Geir-Petter wrote:

I have selected all the features incl. thread.

But the thread will not copy.


That's right. Not in sync. You can see in @hawcad's example that the thread didn't go. Do you not get a warning?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Mirror

Genius
Genius

Yes, I got the warning.

It works in Ordered, so it is OK for me.

 

Cheers

 

Solid Edge 2019

Betreff: Mirror

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So my post wasn't marked as a solution because...?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200