Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirroring a Plane about another Plane

Pioneer
Pioneer

Hello, 

 

I'm looking for a method to mirror a plane about another plane. Does anyone here know how I may be able to do this?

 

Thank you,

Nevin

"The society which scorns excellence in plumbing because plumbing is a humble activity, and tolerates shoddiness in philosophy because philosophy is an exalted activity, will have neither good plumbing nor good philosophy. Neither its pipes nor its theories will hold water." -- John W. Gardner
3 REPLIES 3

Betreff: Mirroring a Plane about another Plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

what's about using a plane surface instead of a reference plane for the first object?

 

This could be mirrored about a reference plane.

regards
Wolfgang

Re: Mirroring a Plane about another Plane

Honored Contributor
Honored Contributor

The best work around I can see is to make two planes offset from the center plane. Then use variables to set the offsets equal to each other (X1=-X2). 

 

I then label each plane (F2), then rename the variables to match.

 

To make that easier, with the variables open, highlight each plane to find the variable for it, then rename that/each planes variable to something you can find.

 

I do this frequently for Plane driven assemblies of sheet metal where I want the 0 point in the center. I end up with planes XP XN YP YN ZP ZN. XP = plane positive along the X axis, ZN = plane negative on the Z axis, etc...

 

Then I set XP=-XN, YP=-YN, ZP=-ZN 

Then If needed XP = X/2

I end up with X, Y, Z incontrol of a centered cube.

Re: Mirroring a Plane about another Plane

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @ncsteinb,

 

Do you need planes, or could you make use of the coordiante system to achieve what you need?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000