Cancel
Showing results for 
Search instead for 
Did you mean: 

Mirroring block affects Block Label alignment...

Experimenter
Experimenter

Very new to SE2D however I'm having a problem.  When I mirror a block that contains block labels the mirrored text gets lowered- it appears that the anchor points for the label change properly just that the graphics for the text are shifted down (this also happens with annotations).

 

I'm really liking what I'm seeing so far but this would be a show stopper for me if I can figure out how to easily work around it.

 

Can anyone shed some insight as to what might be going on here?

2 REPLIES

Re: Mirroring block affects Block Label alignment...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Bill,

This is an odd one!...while I don't use blocks that much, I struggle with why you would mirror them in this case, instead of just dragging off a copy, placing and editing as desired.

Also, probably best asked in the "2D Drafting" forum....in case there are specifics that are not handled the same in the commercial versions.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Mirroring block affects Block Label alignment...

Experimenter
Experimenter
Thanks for the response- I'll repost this down there. These are fixed values that I use over and over to generate wiring diagrams- so I don't want to re-enter the same data every time I do a new diagram.