Cancel
Showing results for 
Search instead for 
Did you mean: 

Modal analysis of sheet metal part only shows 0.000 MHz

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I'm trying to do a quick modal analysis on a sheet metal part and the result is alway 0 MHz.  I modeled a tube in the part environment with the same result.  I have also modeled a simple rod and only get 0.00 MHz.  Is there something wrong with Simulation Express or have I done something wrong for 3 different parts?

 

Kyle 

Kyle Joiner
IPA LLC
ST10 MP1
3 REPLIES

Re: Modal analysis of sheet metal part only shows 0.000 MHz

Gears Phenom Gears Phenom
Gears Phenom

Here are some screen shots.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Modal analysis of sheet metal part only shows 0.000 MHz

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Are you using ST6 or earlier? If so edit your file properties, units, advanced units and change frequency to hertz. The default is Mhz and with a resolution of 3 decimal places this will in most practical cases give a result of 0.
Cheers
Mark

Re: Modal analysis of sheet metal part only shows 0.000 MHz

Gears Phenom Gears Phenom
Gears Phenom

Mark,

 

I'm running ST7.  That did the trick.  Thanks!

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1