Cancel
Showing results for 
Search instead for 
Did you mean: 

Model a wave spring in Solid Edge ST 7

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi All,

 

I have a potential customer that ask me on how to create a wave spring.

 

Is it I need to use some equation in order to create a cylidrical wave shape? Please advices

 
 
 
 
2 REPLIES

Re: Model a wave spring in Solid Edge ST 7

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom
l typically create the cross sections at every peak and valley of the wave and then create a loft between them in ordered mode to maintain the links to the driving sketches.


____________________________________
--Scott Wertel, P.E.

Re: Model a wave spring in Solid Edge ST 7

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

If you have to make a wave spring with several turns you might use a Curve_By_Table to drive helical wavy sketches.  If need be you can also add shim (ie flat) top and bottom faces.

 

Here's one I made earlier.............

Capture.PNG

 

Frank

Edinburgh University