Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeling with Multiple Windows

I am trying to use multile windows when modeling.  Is there a way to show differnt display configurations in each window? and or turn items off in one window and not the other?

 

It seems to only let you change view rotation and turn clipping on and off.  Am I missing somthing?

 

Thanks

 

John

27 REPLIES 27

Re: Modeling with Multiple Windows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think what you are seeing is all you get.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Modeling with Multiple Windows

Honored Contributor
Honored Contributor

Any one license of Solid Edge can only open each single part one time into an occurrence of SE (yes there can be a 1000's of them in the model). If you make a copy of the files and place it in a different directory then you could open both at once using a second occurrence of SE with the same license. But there is no way to get two views that are active on the same model. You can stretch the one view across two monitors, but that does not how I like to work.

 

I made a list of about 50 ER's about two years ago. Only the top 20 got filed, That one was about #45 on my list.

Re: Modeling with Multiple Windows

Creator
Creator

Are you talking about viewports like this? 

Re: Modeling with Multiple Windows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bhaskin

 

 

no I think this is not exactly what was requested.

Multiple views of one and the same 3D document is no problem with SE.

Wether You arrange them side by side or as 4 quadrants, this makes no difference.

But there always are the same configurations visible, exactly the same parts shown, only the zoom area and the view directions differs.

 

I believe, what the original reuqest was, to show different configs, different parts in those windows.

 

And Yes this could be a good enhancement.

 

regards
Wolfgang

Re: Modeling with Multiple Windows

Yes,  I just need to show differnt display configurations (Parts on and off) in each view.

 

Thanks

Re: Modeling with Multiple Windows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @John-Matthews

 

 

I think this will not be possible so far.

 

Multiple windows in SE shows the same situation of the 3D document.

Any changes will be in every window.

 

 

regards
Wolfgang

Re: Modeling with Multiple Windows

I filed an ER.  #8830404

Re: Modeling with Multiple Windows

Honored Contributor
Honored Contributor

The way it should is work is the second copy opened is read only. Then you could inspect with one instance while working in the other. 

 

When some of my model is parts used in another this would really really help.

 

Where this is a common issues is when some core complex parts are being re-designed from one situation to another. 

Re: Modeling with Multiple Windows

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE wrote:

The way it should is work is the second copy opened is read only. Then you could inspect with one instance while working in the other. 



You should be able to do that with a second instance of SE.


Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200