Cancel
Showing results for 
Search instead for 
Did you mean: 

Modelling fully constrained Pipe

Experimenter
Experimenter

What is the right way to model straight pipe in Solid Edge ST8? I am struggling with fully constrained sketches or better said my sketches are not fully constrained

3 REPLIES 3

Betreff: Modelling fully constrained Pipe

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Newbie_designer

 

 

can You giv e a more detailed describtion what You want to do?

 

About which environement are You talking?

ASM, part, 3d sketch, xPresRoute.

 

What do You have so far?

Where are the underconstrains?

 

Do You have a picture or an example doc.

 

 

regards
Wolfgang

Re: Modelling fully constrained Pipe

Honored Contributor
Honored Contributor

What helps the most with achieving fully constrained with ordered sketches is inspect/relations colors. I have it set up so that when all is nailed down, the sketches turn black.

Re: Modelling fully constrained Pipe

Gears Phenom Gears Phenom
Gears Phenom

Maybe this will help. Notice where I click on "Relationship Colors". You're going to want to make sure that is on.

(view in My Videos)

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"