Cancel
Showing results for 
Search instead for 
Did you mean: 

Modifying the Flow Line in Exploded View

Phenom
Phenom

Hi Edgers,

 

relatively simple question - how to modity the Flow Line. Seams to be a quick one but I am stucked.

after studying the Help area I found that there should be an option to change the direction of the flow line like on the attached screenshot:

 

Flow lines.png

 

but I cannot find more arrows to manipulate the line, only have one going along the path line.

Can you tell me how to activate the others please ?

 

(view in My Videos)

 

 

 

2 REPLIES

Re: Modifying the Flow Line in Exploded View

Gears Phenom Gears Phenom
Gears Phenom

there is a difference between Event and Annotation flow lines.

 

If you are trying to modify the event FLow line you need to runt he "DROP" command which converts Event Flwo lines to Annotation flow line which then should edit like you expect.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Modifying the Flow Line in Exploded View

Phenom
Phenom

Hi @Johnson_BigMatt

 

you are the Star !!!

 

thank you,

 

regards,

 

Arek