Cancel
Showing results for 
Search instead for 
Did you mean: 

Modifying the Geometry - HowTo ?

Genius
Genius

Hi all,

 

A very simple and basic question to the specialists:

 

I have an extruded triangle. It is placed within a square area of 500mm side width.

But to have it symmetric I would need the length of 184,62mm on the right side to be changed to 250mm.

I can access the two measures of 500mm, but I cannot access the 184,62mm.

 

What would be the simplest way to make the triangle symmetric with 250mm on the right side?

 

What would make the right hand side measure of 184,62 modifyable like the others?

 

best regards

Hans

 

(view in My Videos)

14 REPLIES 14

Re: Modifying the Geometry - HowTo ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Face relate horizontal/vertical is a way in sync. In ordered, a sketch.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Modifying the Geometry - HowTo ?

Genius
Genius

So there is no way to access the the dimension and change it to 250?

Re: Modifying the Geometry - HowTo ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure why it's reference. Could you upload the model?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Modifying the Geometry - HowTo ?

Genius
Genius

That the asm, are the par's also needed?

Betreff: Modifying the Geometry - HowTo ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hans11

 

 

 

my first and quick answer here would be, why using dimensions to get it symmetric.

use a symmetric relation to say: "Hi, triangle You are symmetric!"

 

This by the way is an old and long used procedere for me, independent wether or not You work synchrous or traditional.

Doesn't matter.

 

Always - and this is my suggestion to any new user and trainee I have with Solid Edge - always first try to make Your geometry good in the matter of geometrical quality, before concern the quantities, what are the dimensions.

A dimension is not the rigth tool to get it symmetric, You have geometrical relations to do so.

 

Another issue I immediateley have seen in Your video.

Why, if You want to have our geometry symmetric, why do You not use the coordinates system right from the beginning to use symmetric relations and even easier DesignIntends.

 

This would make the hole part that easy and flexibel, and this even with less dimensions and formulars.

 

Nevertheless, it also is no problem to do it with dimensions as You have tried it to do.

 

See video.

 

(view in My Videos)

 

regards
Wolfgang

Betreff: Modifying the Geometry - HowTo ?

Genius
Genius

Hi Wolfgang

 

Thank You for creating the video. Unfortunately I can't see, as it is pic saying,

order cannot be executed

 

Your are right. Right from the beginning there would be better means to create it symmetric. But it was a bigger triangle placed on baseplatform. When I tried to minimize it, it became non symmetric and I tried to cure it with dimensions. But I came to the point, where I couldn't modify one of the dimensions, while I could modify the others.

 

By the way there are further issues I don't really understand. Thats the difference between the behaviour of lines and volumes. I can create a par containing a volume with lines on it. But if I import the par file, I only see the volume but not the lines, I would like to use for frames.

 

best regards

Hans

Betreff: Modifying the Geometry - HowTo ?

Genius
Genius

Oh just writing the last point, I found I have the set "lines on" in the asm-file.

Betreff: Modifying the Geometry - HowTo ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hans11

 

 

just uploaded the video again.

 

See it in above post!

 

regards
Wolfgang

Betreff: Modifying the Geometry - HowTo ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hans11

 

 

 

when You talk about "importing a part..." do You think about placing the part into an assembly or create a part copy into another part?

 

Both will work, but depending on the situation I have to give different answers.

 

 

regards
Wolfgang