Cancel
Showing results for 
Search instead for 
Did you mean: 

Module less than 1mm - Engineering Reference Tool

Experimenter
Experimenter

Hi there!

 

I was wondering if anyone could tell me how to draw a set of gears with a module less than 1mm using the engineering reference tool in ST6 assembly?


Whenever I try to change the module to say 0.5mm, the value defaults back to 1mm.

 

Thanks!

6 REPLIES 6

Re: Module less than 1mm - Engineering Reference Tool

Siemens Legend Siemens Legend
Siemens Legend

CJ,

 

If you go to the options page and turn on the Advanced Calculations option you can set the modulus below 1.0 mm
When doing this you have to specify some additional values to make the gear.

 

Hope this helps.

 

Thanks,

 

Art

Re: Module less than 1mm - Engineering Reference Tool

Experimenter
Experimenter

Hi Art,

 

Thanks for your reply, that is very helpful.

 

Unfortunately there doesn't seem to be a similar trick for the bevelled gears...

 

CJ

 

 

 

 

 

Re: Module less than 1mm - Engineering Reference Tool

Siemens Legend Siemens Legend
Siemens Legend
Well rats, you are correct bevel gears don't have this option.

Been awhile since I ran through the bevel gear formulas. Seems like the same options should apply. Would be a good ER.

Sorry this does not help you out.

Thanks,

Art

Re: Module less than 1mm - Engineering Reference Tool

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Did you try Camnetics?  http://www.camnetics.com/geartrax/index.htm

 

I think there is a 10 days trial version from this, it can be useful for you. Very simple to use! Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Module less than 1mm - Engineering Reference Tool

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We have used Camnetics Gear Trax.  You really need it if you are actually designing custom gears.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Module less than 1mm - Engineering Reference Tool

Experimenter
Experimenter

Thank you everyone for your help.

 

I ended up trying two different plugins; eAssistant and Camnetics GearTrax. The former has a similar limitation on the module, but the latter does exactly what I need.

 

Thanks again!