Cancel
Showing results for 
Search instead for 
Did you mean: 

Modyfying Chamfear or round

Pioneer
Pioneer

Hello everyone

 

I'am a new user of SE. Last few yars I worked with SW.

I've problem with modyfication of rounded edges.

 

Example. I rounded five edges. But now I want to have rounded only four.

So. I'am editing definition and I want to deselect one of edges. But I can not to deselect this edge.

How to do this?

 

 

Regards

 

Marcin

 

5 REPLIES 5

Re: Modyfying Chamfear or round

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @SUCHY,

 

This should work exactly as you describe, if you're in "Ordered" mode.....if in "Synchronous", you'd need to select the fillet face[s] that you nolonger want, and delete it/them, as required.

 

 

(view in My Videos)

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Modyfying Chamfear or round

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi:

 

You can de-select one of the rounded edges as shown in video below.

When picking the edge, I kept the Control key pressed:

 

 

This method applies to ordered mode.

The method for handling this in Synchronous is as shown in previous video by @SeanCresswell

   

I hope together you will get the full idea of handling rounded edges.

  

~Tushar

 

 

Re: Modyfying Chamfear or round

Pioneer
Pioneer

Hello Sean

 

Thank You very much for help.

In synchronous mode it works ok.

But in ordered mode it's not possible to do this

Re: Modyfying Chamfear or round

Pioneer
Pioneer

Hello Tushar

 

It works like You described.

 

Thanks for help.

 

Regards

Re: Modyfying Chamfear or round

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Marcin:

  

Since you did not mention the mode, Sean showed you the steps in Sync.

My video shows the steps in Ordered.

I am not sure what really worked for you based on your two replies.

Kindly mark all posts as accepted solutions which worked for you.

You can accept multiple solutions.

  

~Tushar