Cancel
Showing results for 
Search instead for 
Did you mean: 

More draft views

Creator
Creator

Hi All,

 

I've drawn a part using two sketches extruded together as it has to sit on an angle. The part it flat, but has complex splined curves so I don't actually know its exact dimensions hence I need to print a template from which to cut the part.

 

When I try to put it in a draft file so I can print the template, the views I get sare the standard ones of the XY, XZ and YZ planes. The plane I need is not coplanar with any of these.

 

Is there any way I can get a draft view of this extra plane?

Thanks

Sam

1 REPLY

Re: More draft views

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can create a saved view in the model which will then appear when specifying the view to use in Draft.  You can also specify a user-defined orientation if you have a planar face to use to set the orientation.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com