Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

More than one tap in par not showing correctly

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

i'm on update 7. i'll put in more than one tap at a time. when i finish it, only one tap shows and the rest show's as a hole.

 

 

 

16 REPLIES 16

Re: More than one tap in par not showing correctly

Phenom
Phenom

I can confirm that I am seeing the same thing with MP7 on my home laptop. In a shaded model all holes show the thread texture, but only the first placed hole shows the dashed tapped hole in wire frame like your image. More seriously, a drawing shows the dashed tapped hole circle on only one hole also. A call-out placed on one of the other holes properly calls out the thread data.

 

I am seeing this on my home laptop with a non-approved graphics card. I will try it on my work machine and see if the same problem shows up there.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: More than one tap in par not showing correctly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
This is an issue with ST7 MP7 in sequential mode and is an PR.
I recommend to return to MP6 until this is fixed.
regards

JB
SE 2019, VS2017

Re: More than one tap in par not showing correctly

Legend
Legend

Fortunately it's so easy to switch back Smiley Frustrated

Greetings from Germany
Christian Kunkel
https://c-k-m.info

Re: More than one tap in par not showing correctly

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

thanks guy's. it is easy since i just updated my computer.

Re: More than one tap in par not showing correctly

Phenom
Phenom

Well, thanks for this.

I just finished updating 18 workstations to MP7 this morning !

 

Are drawing views affected or is it just in the model ?

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: More than one tap in par not showing correctly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@TDB wrote:

i'm on update 7. i'll put in more than one tap at a time. when i finish it, only one tap shows and the rest show's as a hole.


 

 

Hi there,

 

Your image shows this still within the command edit sequence, so I would see this as expected behaiviour, to show the thread hatchings & depth info, etc, on the primary [or selected - in Synch] hole feature....all else seems to display correctly for me on my system [in all display modes & in draft].....will check parity on my coleagues desktop workstation when I get into the office.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: More than one tap in par not showing correctly

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

that was a Dynamic Edit. didn't matter, they were still screwed up

Re: More than one tap in par not showing correctly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

So you're saying while in Ordered edit mode, you want it to display the rest of the holes in the "group", or "sub-set", with the hatching, etc....?

 

I don't see the model actually not representing what the input is set to though....what am I missing?

 

ST7_PAR_BaseHoleFeatureDisplay.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: More than one tap in par not showing correctly

Phenom
Phenom

Notice how only the lower left hole shows the dashed line for the thread. It does in fact show the texture of a thread, but not the dashed lines. Now, when you drop that model into a drawing, you will get the same thing. Only one hole will show the dashed thread lines. 

 

The intelligence is there: If I place a hole call out on a hole that does not show dashed thread lines, it will recognize the threads in the call out, but won't display the dashes.

 

When you initially place the tapped holes it shows all holes with dashed thread lines properly. But if you edit definition after completing the feature, the dashed thread lines all disappear exceot for the firtst hole placed.

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317