Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: More than one tap in par not showing correctly

Phenom
Phenom

Initial Hole Placement:

Hole Placement.jpg

 

Edit Hole Definition:

 

After Direction Selection.jpg

 

Drawing:

 

Drawing w_ Dim.jpg

 

 

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: More than one tap in par not showing correctly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I can understand the two model views [geometry vs. feature controls],....but the draft view is a regression for sure, of which I can confirm I do actually see this also, BUT, only from an Ordered model....Synch model appears fine in draft.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: More than one tap in par not showing correctly

Phenom
Phenom

Hmmmmm.....maybe it is designed as a way to get us "orderly" people switched over! Smiley Happy

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: More than one tap in par not showing correctly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Has anybody submitted this regression as a PR to GTAC?

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: More than one tap in par not showing correctly

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Does it update if you do a Ctrl+Shift when clicking update views? I have a logged call with assemblies features not displaying, but the force update brings it back. I wonder if this is a similar bug?

Highlighted

Re: More than one tap in par not showing correctly

Phenom
Phenom

Someone said in one of the early posts that it was aknown issue with a PR. I did not see a number though.

 

It is a model issue not a drawing update issue. CTRL-Shift with update does nothing.

 

Bob

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: More than one tap in par not showing correctly

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

the PR is 7394178.

So if you also want to create an IR, you should references this PR.

 

Greetings

regards

JB
SE 2020, VS2017