Cancel
Showing results for 
Search instead for 
Did you mean: 

Movement of a Part from PathFinder to Assembly/ Video

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Started to add parts to the assembly, being away from SE. I forgot the procedure to move after moving from Path Finder.

http://screencast.com/t/AM7wOoheJbM

 

Thanks

Greg

4 REPLIES

Wow...that system performance lag must be hard to live wi...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Wow...that system performance lag must be hard to live with. I see this on my daughters laptop as well...ST4 seemed a little better in this respect.

 

Anyway, what you appear to have done in that video, is choose to edit the part in the context of the assembly, so trying to position the part there will have little or no effect. I suspect the performance lag may be partly responsible for the mis-selection of faces for alignment/mates.

 

If your placing a lot of the same or similar parts, try making a common feature set, [maybe a small cylinder] then use the "Capture Fit" command [look in help for more info] then placing the next instance will be a matter of selecting the target faces, in the corresponding order of mates set. A real time saver!

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Able to Restore

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
This video is from Converter Print2Cad 2014 the video is to convert from 2D
to 3D. I'm courious if able to restore, tried to work back to 3D nothing
doing.http://screencast.com/t/Ruj4IYKaZyO
With this PDF the doc. is in half. Is the doc repairable.
http://screencast.com/t/nrxR2BKUgYzW

I cannot send to community. This information is important There will be an
interview in two week for these doc.

I hope you understand
Greg

Re: Wow...that system performance lag must be hard to live wi...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Where is your original Solid Edge file?


Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Wow...that system performance lag must be hard to live wi...

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
Gone when the computer crashed I lost all files.However, I did save some
files on external drive that's it.
Thanks
Greg