Moving Text Profiles in a sketch back to Ordered

Valued Contributor
Valued Contributor

Hi,

 

A guy at work has 'moved' the sketch profiles of a control panel to Sync.

 

He wanted to just move the instrument/botton/gauge holes to Sync but moved them by accident. 

 

The model has saved now with no backup.

 

Any ideas, i want the text profiles to be editable and not just sketch entities if i was to use project to sketch.

 

Chris

ST8 MP11 / ST9 MP02
5 REPLIES

Re: Moving Text Profiles in a sketch back to Ordered

Phenom
Phenom

After copying the sketch from sync, you will need to start a new sketch in ordered to paste it.

 

~Tushar

Re: Moving Text Profiles in a sketch back to Ordered

Esteemed Contributor
Esteemed Contributor

Hi @ChrisMorgan,

 

This works as @Tushar says, just select & copy the relevant sketch entry in the pathfinder.....to then paste inside a new sketch environment in ordered.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Moving Text Profiles in a sketch back to Ordered

Valued Contributor
Valued Contributor

Saldy all Paste Options are Greyed out when i try and do this!

 

No Solution....

ST8 MP11 / ST9 MP02

Re: Moving Text Profiles in a sketch back to Ordered

Phenom
Phenom

Hi Chris:

   

You need to be in a sketch environment in 'Ordered' for Paste to be enabled.

The screen-grab shows you are in ordered but not clear if you are in the sketcher.

Else you might not have 'Copied' the sketch from sync yet, so the Paste option is grayed out.

    

~Tushar

Re: Moving Text Profiles in a sketch back to Ordered

Valued Contributor
Valued Contributor

Yes, i was see SS, you can only copy 2 types of element at once, Dimension, Sketch elements or Text profile. 

 

So moving them over seperately solved this. 

 

Thanks for the help

ST8 MP11 / ST9 MP02