Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving a Face

Pioneer
Pioneer

I've created a face and can move it with the Steering Wheel, but not with a measurement. Can you check the video and let me know if I'm doing something wrong or there is a way to make it work?

 

Thanks.

 

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

3 REPLIES 3

Re: Moving a Face

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Make sure you are dimensioning to the face you want to move and not an edge.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Moving a Face

Pioneer
Pioneer

Thanks, I just tried and can dimension the face if I select a different point (in this case the edge of the flat panel along the length of the rod), but I want to measure from the axis of the rod. Also I'm not if I understand what you mean as the dimension tool will only select an edge. 

 

 

Re: Moving a Face

Honored Contributor
Honored Contributor

you need to pick (close) the "lock" on the dimension before editing to make it in control.