Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving a Hole

N/A

I've been having issues moving a hole within a part while keeping the center point. Moving up and down fine. Moving left to right always getting a warning.
http://screencast.com/t/iE1HcPIQn
Thanks
Crousie

3 REPLIES

Re: Moving a Hole

Esteemed Contributor
Esteemed Contributor
perhaps you could show a video of attempting to move the hole...


Ken

Production: ST10 MP5
Testing: SE 2019

Re: Moving a Hole

N/A
The first issue is dealing with the steering wheel always chasing and flipping as you can see. Is there a short cut on using the steering wheel? I've been using the shift, and or the Ctrl. Not knowing on how to move the hole with two different parts on top of one another. Also, moving from one hole to another part.
This us the video,
http://screencast.com/t/9Uod7AGh2Z

Re: Moving a Hole

Phenom
Phenom
First of all, where you are trying to move the hole is very unclear from the video. Second, you are getting a warning because of the reason shown in the message at the 0:57 mark in your video. Relationships are being applied to the hole that prevent you from moving it. Have you tried turning off any of the Live rules that control the behavior of the edit? (Bottom rows of buttons on the screen, visible at the 0:57 mark and elsewhere.)
-Dylan Gondyke