11-18-2015 02:31 PM
Hello,
In the past, I made use of the split part command to split parts into linked sub parts. For example, I make installation templates that are used to make drilling holes to anchor our machines to concrete floors. The templates are usually several feet long so I split them up to make the easier to handle. With multi-body, replacing split part, a different approach is required. This is my first venture into multi-body and it seems to be more difficult to work with than split part. For example, I put some oval cutouts in the template halves for handles. In the past, I would create one cutout and then mirror it over to the other side, update the linked parts and move on. Now, I'm finding that multi-body won't let me do that. Am I missing something? Here is an image of the template and you can see the obround cutout I want to mirror. It's a simple part and this was a 5-10 minute job with previous split part tool.
11-18-2015 02:46 PM
Can you drag Split down to the bottom of the tree and then do your mirror above it?
Devide Part is still in the software. Just not on the ribbon.
11-18-2015 02:52 PM
Jason,
I got around the problem by dragging the handle cutout and mirror plane to just below the original protrusion and above the split.
I'm glad you mentioned the split part sitll being in SE. I thought I recalled someone mentioning that in the past. Where is it located?
Kyle
11-18-2015 02:54 PM
Jason,
I meant divide part.
Kyle
11-18-2015 03:06 PM
RMB Customize on the Ribbon.
Seems to me that Devide Part is the same as doing all your multi-body devides at the end of the modeling process.
I don't know the future of Devide Part.
11-18-2015 03:06 PM
Hi Kyle,
As @JasonTitcomb says, it is still inside Solid Edge,.....I get to it via "Command Finder". If you prefer to use this, it only work in Ordered mode.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000
11-18-2015 03:13 PM
Hello,
I had the pull down for customizing the ribbon set to "all tabs" and not "all commands". This many years later, I'm still not liking the fluent interface but that's a Microsoft issue not an SE issue.
Kyle
11-19-2015 03:16 AM
Good to know that "some" SE Icons/Commands are not in the ribbon bar!
I will check all Comamnds under Customise after new SE releases
Yasser
11-19-2015 03:25 AM
Hi Sean,
it seems, it works in Synchronous too. I tried it and it works fine.
Yasser
11-19-2015 10:01 AM
Has anyone else noticed the odd limitation of the split part command? - it doesn't let you split a single body with two solids into two bodies i.e. if you were to extrude two circles to make two separate cylinders (but just one body as far as SE is concerned), you can't split them into two bodies.
Does anyone know a way around this? Obviously my example is trivial - in this case you'd just extrude one, then add body and extrude the other.