Cancel
Showing results for 
Search instead for 
Did you mean: 

Multifunction menù problem in Draft environment

Experimenter
Experimenter

Goodmorning to all.

I have a problem with the multifucntion menù only in the draft environment: when I click on the menù all the buttons of the menù are invisible and I can't work. (see the pic1)

Moreover only in the same environment, when I click on the right corner button, reduce down, all the three buttons (reduce to icon, reduce down and close) disappear(pic2).

Two my colleagues today have the same problem.

All the others environment seems to work fine (pic3).

 

My PC has windows 10 Pro 64 bit

Intel i7-2600 CPU 3,40 GHz

8,00 GB RAM

NVIDIA Quadro 2000 Graphic Card 

Solid Edge ST9 MP3

 

Thanks 

Federigo

3 REPLIES 3

Re: Multifunction menù problem in Draft environment

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

it looks like you have corrupted themes.

Try restart SE and before opening any file, change you current theme to default one.

 

Hope this helps.

 

Ota

Re: Multifunction menù problem in Draft environment

Experimenter
Experimenter

Thanks a lot, you're right!

I'm working with a old Solid Edge theme imported from ST8. I delete all my theme and I made a new theme.

Now it work fine!

 

 

Re: Multifunction menù problem in Draft environment

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You are welcome.

I am glad that it helped.

 

Ota