Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple drawings in single draft File

Pioneer
Pioneer

Hello,

 

       I am trying to put all the drawings of a particular assembly in a single draft file.

 

      But the the callout of the background dosent seem to be working correctly for me.

 

     On sheet 1 i have a different part and the call outs are correct for it but on the second 

 

     sheet i have a different part but it is taking the callout from sheet one.

 

    Any ideas how to fix this.

 

Thanks,

Balaji

5 REPLIES

Re: Multiple drawings in single draft File

Genius
Genius

If you want the part number and title to change from sheet to sheet as the parts change, then in the Property Text, use Named Reference rather than Active Document.  Be sure to select which reference/part you want to pull the information from.  Here is a video...

 

(view in My Videos)

Brian Fritz
Solid Edge Certified Professional
ST10 latest MP

Re: Multiple drawings in single draft File

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I assume that you will group the drawings of a project but be aware that a change of a single part will effect all drawings not only the one where the single part is used.

 

There is a solution called "ProjectPlot". This solution is collecting all drawings from all models in  assembly then you can start printing

 

- print to physical paper

- print each single drawing to single PDF

- print all drawings to single PDF

- etc.

 

Here is a Video about it

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: Multiple drawings in single draft File

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Where can one acquire ProjectPlot?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Multiple drawings in single draft File

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

The online Shop is right now german only so just drop me a e-mail and I will send you all information.

 

http://www.edgeshop.de/

 

Stefan

smitsch@unitec.de
www.all4edge.de

Re: Multiple drawings in single draft File

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Stefan_Mitsch Danke

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200