Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple monitors error

Experimenter
Experimenter

I have the following problem, I have long wanted to arrange a game deck with 2 monitors. I have a gaming laptop asus, pretty powerful. Asus ROG gl52vt - it`s specs. For monitors, I have a similar docking station with 2 DVI and HDMI outputs. When I connect to the monitor, one does not work (optional) only the one that in the settings is selected as the main one. One monitor is an old Siemens with a DVI output, a second new LG 4k. What could be the problem?

1 REPLY 1

Re: Multiple monitors error

Experimenter
Experimenter

I think there may be some troubles with drivers, but it`s not for sure...