Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple slots in one slot feature?

Innovator
Innovator

Why cant i have more than 1 slot in my slot feature? like i can in a hole feature?

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
7 REPLIES

Re: Multiple slots in one slot feature?

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
You are not the first, or the only, person to ask this question. I am hopeful that a new Solid Edge release will enhance the slot command to allow definition of multiple slots in one feature.

Jason

Re: Multiple slots in one slot feature?

Gears Phenom Gears Phenom
Gears Phenom

This will be available in an upcoming release of Solid Edge but not supported as of now.

Re: Multiple slots in one slot feature?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Tushar

 

 

 

are You knowing more than others or are  You looking into Your magic cristal sphere?

 



regards
Wolfgang

Re: Multiple slots in one slot feature?

Community Manager Community Manager
Community Manager

Let's not put anyone with potential insider information in an awkward spot. Let me tell you this:

 

1. It is right at the top of most requested ERs.

2. We take ERs seriously and they are worked on based on popularity (and some notion of doability)

3. Coming soon to a theatre near you...:-)

 

Best,

Dan

Dan Staples
Director, Solid Edge Product Development

Re: Multiple slots in one slot feature?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dcstaples

 

 

great news, and I hope I have read correctly between Your lines Smiley Wink



regards
Wolfgang

Re: Multiple slots in one slot feature?

Gears Phenom Gears Phenom
Gears Phenom

Hi @hawcad

 

I am registered for Solid Edge 2019 beta testing but never got a chance to actually install it - no license requested yet.

The company I work for, Krones AG, is one of the largest users of SE with 1000+ users and they are involved in the beta testing, like many other large customers, in a big way. I have heard our company has been requesting this feature for several years via an ER and it will be included soon - but no idea how soon it would be. Hence my comment - in "an upcoming" version - not the "next" version.

   

[EDIT] And no. I never click the 'I Agree' button on any EULA blindly Smiley Wink

   

Regards,,

Tushar

 

Re: Multiple slots in one slot feature?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

great.

This is a great an good company, what I know in Germany.

And as it sounds in India as well, isn't it?

 

And this sounds as we can hope and expect some changes in that area, especially in connection to that what was mentioned by @dcstaples too.

 

I never ever had the  intention to bring You into troubles, I only was surprised about that info.

But finally we know that there is something in motion.



regards
Wolfgang