Cancel
Showing results for 
Search instead for 
Did you mean: 

Multubody design

Experimenter
Experimenter
I am trying to make frame in multibody. The frame constructed using beams and channels. For each beam and channel separate design body is created. But the gussets/ribs used to connect members are identical in shape. My question is do I need to make no of design bodies for each of gussets even though they are same in geometry. How to copy single design body at multiple location in part environment so it can reflect in BOM in multiples.
3 REPLIES

Re: Multubody design

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Multi-body Design is not intended to duplicate an Assembly file.  My suggestion would be to complete your frame in the part as multi-body without the gussets and then publish your multi-body using the Assembly file option and then in the generated assembly, add your gusset part where needed.  Then you can get your BOM.

 

Another option would be to use the Frame tool in Assembly.  It is going to be much more efficient than trying to use Multi-body in Part, and it will provide a cut lengths for your frame members in the BOM.



Ken

Production: ST10 MP6
Testing: SE 2019

Re: Multubody design

Experimenter
Experimenter
Thank you for your reply, but I had posted frame example to get clarification on more general problem of making duplicate design body for a part.
For example if I am modeling a bracket whose side plates are identical , in that case could I make a design body for single plate and use it at multiple places. in this case if I use mirror command and publish assembly , in individual part file I get two plates instead of one and that doesn't give proper BOM for assembly.

Re: Multubody design

Phenom
Phenom

You still appear to be confusing the multibody process with assembly.

If you have a bracket that has 2 identical side plates, you would model just one of them.

If we then assume you have a base plate for the bracket you would then model that in a separate part file.

Now you create an assembly file and place the base plate and 2 instances of the side plate.

That is the only way to get a correct BOM.

 

If your side plates are mirrored versions of each other you can create one, then in a new part file Insert Part Copy of the first, with the mirrored option.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.