Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NVIDIA K2200 question

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Everyone:

 

I have a very specific query about the NVIDIA "K2200" card.

Below is a screen-grab from the NVIDIA control panel with a K3100M in the system.

 

K3100M.jpg

 

I want to know if "Siemens Solid Edge" is listed and Anti-Alias setting available with a K2200 card too ?

 

If you are using a K2200 card, kindly check if this setting is available.

I need this verified as a requirement for a project before investing $500+ for the K2200 card.

 

Thank you.

 

~Tushar

 

2 REPLIES 2

Re: NVIDIA K2200 question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

K2200

2016-05-09_14-20-45.png



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: NVIDIA K2200 question

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thank you so much Ken !