Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help converting to sheet metal and flattening it.

Builder
Builder

Hi! Could anyone help me convert this to sheet metal and flatten it. I am having difficulty. Materila thickness to be .197(5mm) and all inside radii to be .394 (10mm).

 

Thanks!

3 REPLIES

Re: Need help converting to sheet metal and flattening it.

Community Manager Community Manager
Community Manager

The reason it wont convert/flatten is that that "bend" on the left isn't a true bend. It is kind of a bend and twist. You can see this easily by choosing the Inquire Element command -- it should be a cylinder -- but its not, its a bspline. So the question is -- is this supposed to just be a bent up plate? 

 

If yes -- then you can fix the model using various surfacing and synchronous techiniques and it will convert/flatten. I did this in ST8 -- else I would send you the model.

 

If no -- if it really is supposed to be more than a "strap" in the flat and is a bent then twisted model, you will have to use "Create Blank" to get the shape. This command is only found in Solid Edge Classic and above. 

Dan Staples
Director, Solid Edge Product Development

Re: Need help converting to sheet metal and flattening it.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Dan's diagnose is perfect! It seems this part is coming from catia or pro-e...

 

Here is a short video what I suggest doing "flattenable" part:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Need help converting to sheet metal and flattening it.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Too fast for me Imi.....I was just working on a example video of that very scenario, then spotted your response. As always, another job, VERY well done!

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019