Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Need help extracting part from assembly.

Builder
Builder

So, I have this part that is part of this assembly that happens to be mergerd together as a part. I have no clue how to either delete the large sheetmetal piece and blocks or extract the middle piece from it. It is the part connecting the two I need. Any help is appreciated.

 

Please use this link as the website is giving me errors to upload it.

https://drive.google.com/file/d/0B8ueP-SWSU63VnpFWEhzREpDYTQ/view?usp=sharing

14 REPLIES

Re: Need help extracting part from assembly.

you need to uploard the part file..  the assy is really just a link to the part so there is no data in the assy....

Re: Need help extracting part from assembly.

Builder
Builder

This site will accept neither, but here is a part file.

 https://drive.google.com/file/d/0B8ueP-SWSU63LVpXbGlhUmt1T0E/view?usp=sharing

Re: Need help extracting part from assembly.

ok,

 

so this is one solid body...  I was hoping git may open as multi body but did not...

 

So you could make 100+ cutout as needed to trim away what you don't need and be left with your desired geometry... BUT...

 

Since you are after a sheet metal part here is a little trick...  Barrow the faces of the sheet metal part you desire, thicken that and convert to sheet metal... BAM!!!

 

all can be done in just over 2 minuates

See video here:  http://screencast.com/t/wBkJTBVkT

Re: Need help extracting part from assembly.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Matt, I'm having trouble with screencast. See the attached. How do I make it bigger?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Need help extracting part from assembly.

i dont know why your window is so small but once the video starts there should be an icon on the far bottom Righthand.   you may need to scroll right and down to find it.  if you select that icon it makes the replay fit to screen or full screen..  let me know if that helps?

 

my replay is actually larger than the window size  i have to hit this fit icon so that the entire screen capture is visable in the window.

 

i think it has to do with what resalution i recorded at vs what its viewed at...  but not toatly sure...

 

 the icon is NOT visable until you start playing the video...

 

2015-05-01_1523.png

Re: Need help extracting part from assembly.

this is what i get when i click the video link???  odd huh

2015-05-01_1521.png

Re: Need help extracting part from assembly.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That was it! I had to hit play. Thanks.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Need help extracting part from assembly.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That was some pretty fancy gunslinging there, Matt. Had to watch it a few times and I'm still not sure exactly what you did. 

Is there any way to slow down playback?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Need help extracting part from assembly.

Here you go, made me stay late here at the office on a Friday...

 

But anythign for the Solid Edge Community...  we're all in this together!!!

 

Let me know if this helps at all...: http://screencast.com/t/43zroTaA

 

PS: audio may not be great  no time to play with settings..