Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help in Solid Edge st9

Experimenter
Experimenter

Untitled.pngI need to make a 2d sketch of this in ordered mode, using features such as arc and pattern. 

 

And I have no idea how to start

3 REPLIES

Re: Need help in Solid Edge st9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @MBAmissah,

 

I'm on ST10, so can't offer you a draft file......but this particulat part shouldn't be too difficult to draw.

 

Make your basic geometry just approximated and making use of relationships to help align things, then fillet & trim away the excess line segments, and then go back and place some dimensions on it as required to obtain the actual sizes needed.

 

ST10_DFT_2DProfile.png

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Need help in Solid Edge st9

Experimenter
Experimenter

Wow that's impressive. I'm supposed to use iso part instead of iso  draft so will that affect the procedure?

Re: Need help in Solid Edge st9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MBAmissah, no, makes no difference at all.....the same tools are used.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000