Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Need help with my project

Experimenter
Experimenter

Hey guys, I was trying to create an electric guitar with solid edge with the help of an example model i found on the internet, and i struggled to do the round shape at the edge of the guitar, as you can see below on the images.

How can i do this? Thanks for the help

2 REPLIES 2

Re: Need help with my project

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

There are lots of ways for this, you can use surface modeling or cutout with open profile and etc...

 

Here is a short video about steps:

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Need help with my project

Experimenter
Experimenter

Hi Imics, thank you very much! Your video was very helpful.