Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help with solidwork migration tool

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi guys, 

 

I am trying to migrate solidwork file that I obtained from grabcad to solid edge by using the migration tool. And as soon the process start, this came out;

 

 Error.JPG

 

Can anyone please advise me to solve this thing? Thanks

9 REPLIES 9

Re: Need help with solidwork migration tool

Phenom
Phenom

Could you upload your SW file?

Re: Need help with solidwork migration tool

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi, 

 

I have attached the solidwork file. I'll be glad if you can help

Re: Need help with solidwork migration tool

Valued Contributor
Valued Contributor
Pure guess, do you need to run the program with admin privileges? Guy

CAD/CAE Manager
SE2019 MP5

Re: Need help with solidwork migration tool

Phenom
Phenom

I tried it using Solid Edge ST5 and it doensn't work.

 

Then I used "SW2SE.exe" from Solid Edge folder. It creates the Folder IMPORT but without any content!

 

translation.jpg

Re: Need help with solidwork migration tool

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Is the problem about the migration tool or you just want to import the SW Grabcad assembly into Solid Edge. I am able to open the "pompe hydrailique.SLDASM" in SE using the Open command.

  

Also, using SW2SE.exe was successful in my case and I have attached the resulting parasolid if it is of any help to you.

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

 

Re: Need help with solidwork migration tool

Phenom
Phenom

I can't open it Smiley Sad

Re: Need help with solidwork migration tool

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

@YD wrote:

I can't open it Smiley Sad


SW or X_T ?

I used ST 8

Re: Need help with solidwork migration tool

Community Manager Community Manager
Community Manager

First question is -- why are you using SolidWorks Migrator for this? SW Migrator is designed for large scale migrations of SolidWorks to Solid Edge and requires a SolidWorks seat (do you have one?)  If this is just a SolidWorks file from GrabCAD just use "File Open" from inside Solid Edge.

Dan Staples
Director, Solid Edge Product Development

Re: Need help with solidwork migration tool

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Dan Staples,

 

Thank you for your clarification. 

Is it because i don't have Solidworks seat causing my migration to fail? As it state i dont have sufficient privileges for this operation.