Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Edgers,


we have found following problem when creating a new part or sheet metal document.

 

independed what geoemtry You have (a single block, a tab, a cylindar) and which material You select, after updating the physical properties any value keep 0 (zero.

That means no volume, no area no mass

 

Any checks about Auto-Update, Update on Save etc. are set to Yes

 

Solid Edge Version is ST9 MP11 and Win10 with Creators Update!

 

The user claims that he thinks this behaviour occurs since the Win10 update

 

Could this be verified?

 

 

regards
Wolfgang
16 REPLIES

Re: New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad, I'm not seeing that. A new part has those properties after I create a feature and update physical properties.

Edit: I don't the have the Win10 Fall Creator's Update though. And I'm on ST10 so this info may be useless.

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

 

this is the same what I personall can see.

 

But I also do not have the Win 10 update installed and I'm also using ST10

So I hope, that there is anybody out there, having ST9 and Win10 with Update who can confirm that there are problems or there are not

 

 

 

regards
Wolfgang

Re: New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad, It turns out, much to my dismay, that some of us do have the Win10 Fall Creator's update, me included.

The mass props are ok but we are seeing the dialog slowdowns in SE. Our networking guys installed the updates last week even though I expressly asked that they not include that one. People!

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: New parts physical properties mass is 0

Valued Contributor
Valued Contributor

Hello Wolwgang and Bruce,

 

In October I did install ST10 MP1 on my production desktop  with W7 64bit  Ultimate with all updates (exceptt W10 push junk) and on my home laptop with updated W10 64bit Pro 1709 with all updates upto KB4058043, except one from today 2018-01-04, KB4066892.

SInce then I have not touched Se, working with my SolidWorks 2017 only.

 

After reading your post I did check both computers and seen the following:

ST10 MP1 W7 -  New SE par,   Physical Properties Update Change - OK,   Mass = 0,    after Update call Mass = 0

                       -  New SE psm, Physical Properties Update Change - OK,   Mass  = OK, after Update call Mass = OK  

 

ST10 MP1 W10 - New SE par,   Physical Properties Update Change - SE will Crash,   Mass = 0

                         - New SE psm, Physical Properties Update Change - OK,   Mass  = OK, after Update call Mass = OK

 

After installing SE MP3 on both computers and being forced to restart laptop with todays KB4066892 update, reboot etc, results ar the same on the both computers as above.

 

SE Log text is:

14:18:42.448 [ERROR|0x0760] Src\Ui\ImplicitParentWindow.cpp:28 | Exception: COM automation exception: Unspecified error (80004005) - (null) at Src\Ui\ImplicitParentWindow.cpp:18
14:18:44.206 [ERROR|0x0760] Src\Ui\ImplicitParentWindow.cpp:28 | Exception: COM automation exception: Unspecified error (80004005) - (null) at Src\Ui\ImplicitParentWindow.cpp:18

 

 

Milan Wendl, MEngSc, P.Eng.
AAA Engineering, Canada
ST10, SolidWorks Premium 2018

Re: New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@milanw, You don't say whether these new parts have any features.

Edit: And I'm confused by your "0" and "0K". Are you meaning zero and zero kilograms or Okay?

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: New parts physical properties mass is 0

Valued Contributor
Valued Contributor

Sorry Wolfgang for the typo in your first name, as the slowakische deutsche from Pressburg, on my paternal grandfather side I should know better.

 

Milan Wendl, MEngSc, P.Eng.
AAA Engineering, Canada
ST10, SolidWorks Premium 2018

Re: New parts physical properties mass is 0

Valued Contributor
Valued Contributor
Off course they have features, I pay for Solid Edge continuously since V7.
0 = Zero
OK means that I get realistic numerical value for mass.
Milan Wendl, MEngSc, P.Eng.
AAA Engineering, Canada
ST10, SolidWorks Premium 2018

Re: New parts physical properties mass is 0

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@milanw, Hey, no offense intended. I don't know you, you didn't say, so I had to ask.

Bruce Shand
ST10 MP10 - Insight - Win10 - K4200

Re: New parts physical properties mass is 0

Valued Contributor
Valued Contributor

ST10 laptop with W10 74bit Pro crashlog file and the screen shot showing SE crash and W10 updates at that time are in attachments.

Milan Wendl, MEngSc, P.Eng.
AAA Engineering, Canada
ST10, SolidWorks Premium 2018