Cancel
Showing results for 
Search instead for 
Did you mean: 

New to Simulation

Builder
Builder

I have this simplified axle. I wanted to know if it could handle taking a 800 lb load. So the interior blocks represent where it will be mounted and the exterior blocks represent the wheels. Now, I applied a load of 400 lb to each end. The report I generated says I get a F.S. of approximately 2.5. I havent had strengths of materials in while and was wondering if this is an accurate simulation and 800 lb would be ok as a load. I am refreshing strength this semester and continuing my degree in ME. I am a year or so removed. Thanks!

1 REPLY 1

Re: New to Simulation

Builder
Builder

Maybe run the sim and give me some constructive criticism.