Cancel
Showing results for 
Search instead for 
Did you mean: 

No acces to "Learn Solid Edge" from the program

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I had installed Solid Edge ST10 without any MP.

I have it in Spanish in two diferrent computers.

 

On one of them I can acces to the learning centre without problems. With the other one an error appears: "these place is not safe"

I cannot acces either from chrome or from explorer.

 

¿There is anything I can do?

 

Thank you!

2 REPLIES 2

Re: No acces to "Learn Solid Edge" from the program

Valued Contributor
Valued Contributor

check your browser settings, unless it is a company company computer.  It seems that there is a security setting(s) that are in place to not allow access to that website.

Re: No acces to "Learn Solid Edge" from the program

Siemens Phenom Siemens Phenom
Siemens Phenom

This is a known issue that we are currently working to address:  See this post:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Web-server-help-failure/m-p/436575/...