Cancel
Showing results for 
Search instead for 
Did you mean: 

Non-Solid Part

I'd appreciate some guidance on the best way to fix this part. I imported a STEP file and one surface is missing. I'd like to replace the missing surface and solidify the part. I created a BlueSurf to replace the missing surface but the "Stiched" command was greyed out so I can't figure out how to turn it into a solid. What am I doing wrong?

 

non-solid_part.jpgNon-Solid Part 

 

 

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10
4 REPLIES 4

Betreff: Non-Solid Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @David_McMahon

 

 

 

Yes this is acting a little bit strange.

 

I just copied Your surfaces (oops forget that I deleted the round at top - please add it again Radius 0.031)

 

From those copied surfaces I created a BlueSurf and for testing a connection surfcae.

And - but traditionla only - those can be stitched together into a single solid

 

But as mentioned, I do not understand fully, why Se shows such a behaviour.

 

 

regards
Wolfgang

Betreff: Non-Solid Part

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

There seem to be some inconcistencies with the edges,  can't see why, but increasing the heal and stitch solves it also

Betreff: Non-Solid Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Kaak

 

 

I didn't need to heal it anyway.

The problem IMHO more or less is coming either from Sync or from import into one single body

 

 

regards
Wolfgang

Betreff: Non-Solid Part

Hawcad and Kaak,

 

I greatly appreciate your help with this. Both of your suggested fixes were helpful in solving the problem.

David McMahon
Solid Edge 2019
HP Z2 Mini, Windows 10