Cancel
Showing results for 
Search instead for 
Did you mean: 

Non-uniform pattern - Synchronous

Valued Contributor
Valued Contributor

See figure.

patterns.png

 

As you can see in the picture ...
This is a part.
I made a circle with different lengths.
I want to process it as a pattern.
The length is each ...
Is there a way to pattern it ... synchronous.

 

file Attach

 

7 REPLIES 7

Betreff: Non-uniform pattern - Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

can You explain more in detail what exactly You want to achieve?

 

 

regards
Wolfgang

Betreff: Non-uniform pattern - Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

what's about creating the first frame piece with the proper ends and then simply copy it using the steering wheel.

Afterwards You can change any single item as You need it.

 

 

regards
Wolfgang

Betreff: Non-uniform pattern - Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

see video what I would do in such a case

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

regards
Wolfgang

Betreff: Non-uniform pattern - Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

 

and here another couple of hints/infos regarding Your design request.

 

  • You also can use the "Duplicate Feature" functioinallity which came with ST9 - but this only will be a traditional function, nevertheless it is a great tool exactly for such requests.
  • You either can do it with coordinate systems or with a block sketch
  • Or You also can do it with a curve pattern!
    Yes this will work if You use a zigzag line sketch and this endpoint of line segments.

 

  • Or  You will use table pattern functionality - also came in with ST9

 

You see there are more than one possibilities to use for achieving the given request.

And everyone of them is good and strong.

It is Your choice which one You will prefer

 

 

regards
Wolfgang

Betreff: Non-uniform pattern - Synchronous

Valued Contributor
Valued Contributor

Thankyou hawcad..

 

It's not the way I want to go.
Thank you for suggesting various methods.

I want to pattern only the extruded parts ...
It's a pipe structure.
I wanted to pattern the protruding part because all the corners were later protruded after the green.

Let's try different things.

Betreff: Non-uniform pattern - Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Hclee

 

 

so I cann't follow You with what You request and what Your last answer is.

 

 

You will never be able to pattern something what afterwards is not equyl to the origin.

 

You only can pattern the cutouts and I have given You several methods to do so.

 

If You want to deal with the extrusions, I don't see any way to use a pattern,since every piece of the beam is different.

 

And I also cann't understand why You do not want to use one of this pattern methods I mentioned.

 

 

By the way, I think that any answer - regarding Your other post of the weekend (Synchronous) - would be fine for everybody who has taken his time to seat down on Saturday and Sunday, answering Your question and trying to help.

 

regards
Wolfgang

Betreff: Non-uniform pattern - Synchronous

Valued Contributor
Valued Contributor

Yes I am always thankful ... ^^