Cancel
Showing results for 
Search instead for 
Did you mean: 

Not all threaded holes being shown as threaded - only first hole - ST7

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Is there a setting that controls whether all threaded holes are shown with hidden lines in drafting? As in figure below, only the 1st hole of the feature is being shown as threaded (all the holes are from a single step in the model). I have tried new hole steps, changing the hole size - and metric / inch, new hole steps, all with same result. I would rather all the threaded holes appear as threaded. Do the Edge masters have any ideas?

 

Thanks.

 

Capture.PNG

 

2 REPLIES

Re: Not all threaded holes being shown as threaded - only first hole - ST7

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This known bug has been covered here: 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/More-than-one-tap-in-par-not-showing...

Apparently it has been fixed in MP8.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Not all threaded holes being shown as threaded - only first hole - ST7

PLM World Member Pioneer PLM World Member Pioneer
PLM World Member Pioneer

Thanks for the info. I updated to ST7 MP8 from MP7 and the problem seems fixed. Draft didn't update correctly right away - had to go into the part and create some dummy holes and that seemed to fix things but not really sure what I did that triggered the MP8 fix. However, it does now seem fixed.

 

Thanks bshand.