Cancel
Showing results for 
Search instead for 
Did you mean: 

Not allowing to cut all the way through

Experimenter
Experimenter

I am trying to cut out a sketch that I projected from an assembly. When I go to use the extrude comand and use cut it gives a zero surface error when I try to go all the way through. The part file is attached. Thank you for the help!!

3 REPLIES

Re: Not allowing to cut all the way through

MLombard
Retired

I'm having trouble opening the file, are you using a student edition?

 

Anyway, try moving the lines that are right on the edges of the part so that they hang off the part a little. A very tiny sliver can cause the zero thickness error. If you search that term on the forum, you'll find other cases where this happens, and how to avoid it.

Retired Community Manager for Solid Edge. This account is no longer active.

Re: Not allowing to cut all the way through

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I attempted what Matt suggested and it didn't help although I think I pinpointed the area it's going zero manifold. You could try moving the sketch line which defines the cut here. Not sure why you couldn't open it, Matt.

HEAD1.PNGHEAD2.PNG

 

That's about as far as it would go before it gave an error.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Not allowing to cut all the way through

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

As my friends mentioned you will get a zero thickness wall... You can cut it out from two steps.

 

Here is a video:

 

BR,

Imics
http://solidedgest.wordpress.com/