Cancel
Showing results for 
Search instead for 
Did you mean: 

Nothing works

Not applicable
Looks like I was a bit too hasty in my judgment. Will this program run on windows 7 64 bit?

It worked twice, now splash screen runs, a blank sheet appears with application and quick access buttons that do nothing. The help button on the right when pressed gives the message "you do not have a valid licence to use this command" Nothing appears if you press "New" and try to use any of the tabs on the menu.

Cheers

Bob
14 REPLIES

Re: Nothing works

Not applicable
Bob,
I saw your previous comment about using a tablet.
Are you trying to run the software through the tablet?
Will the software run properly using the keyboard and mouse only?
Regards,
Rick B.

Re: Nothing works

Not applicable
No Rick, I have'nt tried the tablet yet.

Bob

Re: Nothing works

Not applicable
Was the software working properly and then something change so that it no
longer works properly.
I am trying to undestand if the problem existed under default conditions.
Rick B.

Re: Nothing works

Not applicable
Was the software working properly and then something change so that it no
longer works properly.
I am trying to undestand if the problem existed under default conditions.

Rick B.


Hi Rick, after three re-installs, now works, so far so good.

Thanks for your help. Lets hope it keeps going, it's a great program, easy to get to grips with.

Are there any symbol libraries and templates available?

Cheers

Bob

Re: Nothing works

Not applicable
Bob,
I am glad you got it running.
There is a block library in the product.
Lok for the 'Sample Blocks' folder in the product installation folder.
There is also a 'Template' folder there as well.
Regards,
Rick B.

Re: Nothing works

Not applicable
Bob,
I am glad you got it running.
There is a block library in the product.
Lok for the 'Sample Blocks' folder in the product installation folder.
There is also a 'Template' folder there as well.

Regards,
Rick B.


Hi Rick

OK, so the third installation did not completley reinstall. I must have missed some of the original files when i uninstalled, or maybe registry entries. I will do a very careful purge of the system and do another install.

i have installed completely on another pc with XP and no problems, it's just windows 7 thats giving grief. Typical microsoft!!

Thanks Rick

Bob

Re: Nothing works

Not applicable
My best advice is to disable the UAC on Win 7 when you install the software.
Rick B.

Re: Nothing works

Not applicable
My best advice is to disable the UAC on Win 7 when you install the software.

Rick B.


Great minds etc. Did that and all seems to be working as it should be. Still cannot get the tablet to work, but that is a combination of USB/Serial windows 7 driver problems, but I shall do my work on the XP machine where the tablet works faultlessly.

Many thanks for all your help

Bob

Re: Nothing works

Not applicable
Is it win7 pro or Ultimate by any chance? Those are supposed to have an XP emulator that people have said works really well (haven't used it myself).