Cancel
Showing results for 
Search instead for 
Did you mean: 

Nudging Graphics

Not applicable

Good Evening (At least it is here in Aussie)
After inserting a graphic into a drawing is there any way of nudging it into position
in small increments by using the keyboard. It is very hit and miss with the mouse.
Many thanks
Geoff

1 REPLY 1

Re: Nudging Graphics

Not applicable
Geoff,
If you used Insert Image for the graphic, you can display the border of the
image. Then place dimensions between the border of the image and other
geometry. Modify the dimensions to move the image to a specified position.
Delete the dimensions when finished.
Regards,
Rick B.