Cancel
Showing results for 
Search instead for 
Did you mean: 

Number of Holes in drafting

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi,

 

Anybody have an idea on how to automatically come out the number of holes using annotation?

 

Let say I have a part that have 6 counterbore holes (generate using hole wizard) and I would like to do annotation for only one holes since the holes are the same. But the annotation already mention the total number of holes in that part.

 

For now I put it manually from dimension, is it any other way that can do automatically? 

refer the attachment

12 REPLIES

Re: Number of Holes in drafting

Phenom
Phenom
You have to wait for ST9 to do that.

Re: Number of Holes in drafting

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
is it true in upcoming version they will be function like this?

Re: Number of Holes in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there @Arisy,

Pretty sure there is a work around, where you have to expose the quantity in the variable table, to then access in the callout.

It shouldn't have ever been this hard!
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Number of Holes in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Arisy wrote:
is it true in upcoming version they will be function like this?

I'd like to reiterate that question. Is this function going to be in ST9?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Number of Holes in drafting

Siemens Genius Siemens Genius
Siemens Genius

Yes. Dropped at the SEU2015 ST9 sneak peeks session.

 

ST9HoleCount.jpg

---
Aditya Gurushankar
Manager, Solid Edge Planning

Re: Number of Holes in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@AdityaG, Thanks. Guess I missed it.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Number of Holes in drafting

Legend
Legend

Will this require the holes to be all put in a single hole feature or does it just add up holes of the same properties?

 

I ask because I tend to do a single hole and pattern it out as a second step.

Re: Number of Holes in drafting

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Good question!

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Number of Holes in drafting

Siemens Genius Siemens Genius
Siemens Genius
There are a few options - you will be able to count all similar holes in a part, on a face or in the same direction.

Your patterned case will be handled.
---
Aditya Gurushankar
Manager, Solid Edge Planning