Cancel
Showing results for 
Search instead for 
Did you mean: 

Numerous Active Bodies

N/A

I'm showing 3 active bodies and I only want one active, check protrusions all the same.
http://screencast.com/t/5DdpFCH44

Thanks
Crousie

6 REPLIES

Re: Numerous Active Bodies

Esteemed Contributor
Esteemed Contributor
Struggling to recreate your problem based on the image.....can explain a little more of what your trying to do, and the point the problem is encountered?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Numerous Active Bodies

N/A
Crousie,
I agree with Sean that your description is vague. Please try to post more detail or a video.
If you are selecting from the PathFinder you will select the features as a select set.
If you only intend to edit one set of faces simply select them directly from the graphical display.
???

Re: Numerous Active Bodies

N/A
I was understanding only one active at a time. Looking at the Solid Bodies some bodies are missing, Protrusions not working properly.
http://screencast.com/t/g9btZINu

Re: Numerous Active Bodies

N/A
you've only captured a very narrow viewing window in the video. we need to see your pathfinder and the expanded bodies collector to see the multiple bodies...
additionally a little understanding on what you are trying to accomplish would be helpful... i see you randomly clicking on faces and using quickpick but i dont follow what your objective is?

I'd like to help you out but need to see the whole picture and understand what it is you are trying to accomplish.

Re: Numerous Active Bodies

N/A
I think I have every thing you need to see what the issue is. The parts to the right are the ones that were active and had to redo to make not active. Now this is the issue... I've tried every ways from Sunday to fix.
http://screencast.com/t/yBnMP1gqnx

Re: Numerous Active Bodies

Esteemed Contributor
Esteemed Contributor
Crousie,
It appears to me. that you may benifit from modeling in and assembly environment, using the "Create Part In-Place" method ....have look through the help file for more on the topic.


Also, be careful that your design doesn't have the "Non Manifold" condition being used, by way of circle-to-circle tangent contact. This doesn't matter at sketch level, but is game over for modeling parts.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000