Cancel
Showing results for 
Search instead for 
Did you mean: 

OCCURENCE PROPERTIES ISSUE

Gears Phenom Gears Phenom
Gears Phenom

I'm noticing that when I have an occurence property of a subassembly set to not show up in the parts list, then I transfer that subassembly out to a higher level, I can no longer successfully change that occurence property to show up in the parts list. I can bring the subassembly in again and set the occurence properties as I like, but not for the original occurence. Anybody know how to fix this, as I've got quite a number of relationships on this already, not to mention some exploded views, and I'd prefer to not have to redo all of it.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
9 REPLIES 9
Highlighted

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

do You have a video to show what exactly You are doing to get this behaviour?

 

Thanks

 

regards
Wolfgang

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Phenom Gears Phenom
Gears Phenom

Sorry dude, no. What I did was I had an assembly (A), which contained a few sub assemblies. Inside one of those subassemblies (B) I had another subassembly(C). I had assembly (B) open and had from there changed the occurence properties for subassembly (C) to not show in parts lists. Then later on I transferred (C) from (B) out to assembly (A). Then after making a number of relationships and explosions and such, I realized that (C) wasn't showing up in my parts list, and now I cannot change it's occurence properties to show up in parts list. When I try it doesn't stick. I can bring it in again and change it fine, but not change them for the original.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sounds like you've encountered another bug. For your specific problem maybe a workaround is to rename or copy the C assy to another name and do a replace? Maybe a two step replace with the new C then back to the old C? Just a thought.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

OK, tried to rebuild this situation and here (ST9-MP1) I was able to change the occurency property for BOM to Yes back even in the top assembly

 

EIther I did a different approach or it has to do with Your assembly structure or the right to it.

 

regards
Wolfgang

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Phenom Gears Phenom
Gears Phenom

I tried that. No dice. I was thinking maybe transfer the subassembly back into the assembly it was in when I changed the occurence props, then change them, then transfer back but I'm pretty sure if I do that I'll lose my relationships and my explosions and all. I'm now thinking I'll just do some fakery like just have two instances in my assembly and hide one from the view properties or something. That way my balloons will stay linked in most views just not in my explosions.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: OCCURENCE PROPERTIES ISSUE

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Are you using the new Custom Occurrence Properties?

Or did you accidentally click the Add Custom Occurrence Properties buttton?

Not too sure why this would cause the problem though.

 

LMGi
www.TLMGi.com

Betreff: OCCURENCE PROPERTIES ISSUE

Good afternoon,

 

When trying to change the occurence properties, do you do it in the sub assembly self or in the top assembly?

 

Regards,

Theodore

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3

Betreff: OCCURENCE PROPERTIES ISSUE

Gears Phenom Gears Phenom
Gears Phenom
I have tried both. From within the top level, from inside the subassembly, I've also tried selecting occurence props for the entire top level then scrolling to the one in question, I've tried selecting just the subassembly occurence props and changing it standing alone.
Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Betreff: OCCURENCE PROPERTIES ISSUE

Well, that is strange. We just had the same issue where changing the occurence properties in the sub assembly level wouldn't stick.

 

However, from the top assembly level the changes do stick.

 

Regards,

Theodore

 

Capture.JPG

Kind regards,
Theodore Turner

Solid Edge 2019 MP6
Teamcenter 11.3