Cancel
Showing results for 
Search instead for 
Did you mean: 

OT- 3-D printed Shelby Cobra

Phenom
Phenom

This is wild stuff... 500 to 1,000 times faster. This is getting very cool, yet part of me is scared!

 

"The team took six weeks to design, manufacture and assemble the Shelby, including 24 hours of print time. The new BAAM system, jointly developed by ORNL and Cincinnati Incorporated, can print components 500 to 1000 times faster than today’s industrial additive machines. ORNL researchers say the speed of next-generation additive manufacturing offers new opportunities for the automotive industry, especially in prototyping vehicles."

 

shelby_hr-1.jpg

 cobra 8_0.jpgcobra 9_0.jpg

http://www.ornl.gov/ornl/news/news-releases/2015/3-d-printed-shelby-cobra-highlights-ornl-rd-at-detr...

7 REPLIES

Re: OT- 3-D printed Shelby Cobra

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Definetely a cool concept.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: OT- 3-D printed Shelby Cobra

MLombard
Retired

I'm interested in how thick they have to make the material to have something with practical strength.

 

I once took a scaled down model of a Cobra, scanned it with a cheap desktop scanner, and then modeled surfaces over the scan data. I love the shape of these cars. I'd love to drive one one day.

 

With 3D print, you can print mesh models from subdivision modelers where it's so much easier to make organic shapes, and the heroic effort involved in NURBS modeling isn't even an issue. We CAD guys look at shapes like this in envy (or at least I do) because I know how much effort I'd have to put into making something like that with surfacing features. With sub-d tools, its much easier.

 

The original article is very interesting. I wrote a blog on the original Strati car Local Motors made with the same Cincinnati/Oak Ridge Labs machine. http://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Cincinnati-Incorporated-Machine-3D-Pr...

Retired Community Manager for Solid Edge. This account is no longer active.

Re: OT- 3-D printed Shelby Cobra

Phenom
Phenom

Not 3D printing, but in the same rapid-prototyping vein, and equally as fascinating to me. Especially because the premise is so simple!

 

 

 

 

 

-Dylan Gondyke

Re: OT- 3-D printed Shelby Cobra

THATS SWEET!

 

I was unaware of this new technology... 

 

I can clearly see it's usefullness and it's potential

Highlighted

Re: OT- 3-D printed Shelby Cobra

@SeanCresswell have you seen this yet?  super cool!!!

Re: OT- 3-D printed Shelby Cobra

Phenom
Phenom

Matt... everyone knows that Sean is "super cool"  Tell us something we don't know!

Re: OT- 3-D printed Shelby Cobra

Phenom
Phenom

My personal is not the Cobra but the Jaguar XK-140 or 150.

 

But I have to admit that Corba has some beautiful curves too!