Cancel
Showing results for 
Search instead for 
Did you mean: 

Obsolete to in Work

Genius
Genius

Is it possible to change a part file from Obsolete to In Work?

 

A mistake has been done.

 

 

 

Solid Edge 2019
15 REPLIES 15

Re: Obsolete to in Work

Phenom
Phenom

Work around:

Save as (different name)

delete part

rename copy to original name

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: Obsolete to in Work

Gears Phenom Gears Phenom
Gears Phenom

not directly,  but there are some tools floating around to do so...

 

see this thread. https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/Status-Changer-for-ST-10/m-p/442679

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Obsolete to in Work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Here's a direct link to the barham site:

http://barhamsoftware.com/SE_Tools/index.htm

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: Obsolete to in Work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Geir-Petter

 

 

 

I also have found an old macro for chaning the status

Hope it helps

 

 

regards
Wolfgang

Betreff: Obsolete to in Work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@hawcad, I think that's the Barham macro linked to in the Barham website. At least it's the exact same name and file size.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: Obsolete to in Work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @bshand

 

 

this could be, it was used many years ago,
but we have written our one tool for that with a couple of more functions integrated.

 

 

regards
Wolfgang

Betreff: Obsolete to in Work

Genius
Genius

Hi,

I tried the program, but it did not change the file status.

Maybe its not working with Solid Edge 2019.

 

 

 

Solid Edge 2019

Betreff: Obsolete to in Work

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Did you follow @hawcad's suggestion from the linked thread from @Johnson_BigMatt?

 

As follows:

But on the other hand - see several other posts here regarding to the same issue - install the extra "View & Markup".

Even if You don't need it, it brings the 32bit set of API calls back and all the macros can be executed without any problem.

 

My question is that though this worked with ST10 will it still work with 2019?

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Betreff: Obsolete to in Work

Genius
Genius

OK,

I will install View & Markup.

I think this will solve the problem with StatusChanger

Solid Edge 2019